Produkty: AS-B, AS-P, Project Configuration Tool
Funkcje: Lokalizacja
Wersja produktu: 3.3, 2022
2021-07-23

Automation Server – Date & Time View

Use the Date & Time view to configure the automation server time and time zone.

 
action_zoom_plus_stroke Date & Time View
Rysunek: Date & Time View

Tabela: Date & Time View

Component

Description

Network time synchronization

Select to synchronize the automation server clock with a network time server.

Authenticate Network time synchronization

Select if you want to use authenticated network time synchronizing.

Primary time server

​Type the address to the primary time server to which the shadow automation server date and time object synchronizes its clock.

Secondary time server

Type the address to the secondary time server to which the shadow automation servers' date and time object synchronizes its clock.

Key id

Type the ID of the authentication key for the primary time server.

Key id

Type the ID of the authentication key for the secondary time server.

Key value

Type the password for the primary time server.

Key value

Type the password for the secondary time server.

Manually adjust date & time

Select to manually set the automation server clock.

Local date & time

Enter the date and time you want to set the automation server clock to. This time is displayed in automation server local time.

Predefined time zone

​Select the time zone the EcoStruxure BMS server belongs to.

Custom time zone

Select to manually define the EcoStruxure BMS server time zone.

Description

Type a description or name for the customized time zone DST settings.

UTC offset

Select the time difference the time zone has from UTC in the hours and minutes boxes.

This custom time zone uses daylight saving time

Select to enable the daylight saving time settings for the custom time zone.

Time adjustment

​Select the time adjustment, in minutes, for the daylight saving time.

Month - Start

Select the month that daylight saving time starts.

Week - Start

​​Select the week of the month that daylight saving time starts.

Day - Start

Select the day of the week that daylight saving time starts.

Time - Start

Select the time that daylight saving time starts.

Month - End

Select the month that daylight saving time ends.

Week - End

Select the week that daylight saving time ends.

Day - End

Select the day of the week that daylight saving time ends.

Time- End

Select the time that daylight saving time ends.

  • Time and Time Zone Configuration in Automation Server
  • Network Time
  • List View Toolbar
  • Device Discovery View
  • Communication View