Backup the EcoStruxure Building Operation software license files on a regular basis. To back up the license files, copy all files in the folder to an external resource. Backups are useful if the hardware or the operating system malfunctions.
Backed up licenses can only be restored on the same License Server that the files were backed up from. If you plan to move the licenses to another License Server, you first must return the licenses to the License Activation Server and then activate them on the new License Server.
有关更多信息,请参阅 EcoStruxure Building Operation Software License Return
.
The license files are located in: \ProgramData\FLEXnet in Windows.
The restored licenses files may on rare occasions be considered damaged by the License Server. If so, they must be repaired.
有关更多信息,请参阅 EcoStruxure Building Operation Software License Repair
.