earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
3
用户界面

用户界面


产品: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
功能: 基本功能
产品版本: 1.8
2016/10/13

Backup Options Dialog Box

Use the Backup Options dialog box to select the SmartStruxure server and the type of data that you want to back up. You can also enter a unique file name for the backup set.

 
action_zoom_plus_stroke Backup Options dialog box
图: Backup Options dialog box

表格: Backup Options Dialog Box

Property

Description

Backup set name prefix 

Type the text that you want to add to the beginning of the file name to help identify the backup set.

Backup set name suffix 

Type the text that you want to add to the end of the file name to help identify the backup set.

 
action_zoom_plus_stroke

Click to include all the listed SmartStruxure servers in the backup operation. You can also manually include or exclude a SmartStruxure server using the Include check box.

 
action_zoom_plus_stroke

Click to exclude all the SmartStruxure servers selected for the backup operation.

 
action_zoom_plus_stroke

Click to add the same backup set description entered for one SmartStruxure server to all the other backup sets, such as Final Configuration.

 
action_zoom_plus_stroke

Click to add the same content type chosen for one SmartStruxure server to all the other backup sets, such as Configuration only.

 
action_zoom_plus_stroke

Click to add both the backup set desciption and content type chosen for one SmartStruxure server to all the other backup sets, such as Final Configuration and Configuration only.

Server name  

Displays the name of the SmartStruxure server.

Include

Select the SmartStruxure servers that you want to include in the backup.

Backup set name

Displays the name of the backup set that you entered.

Backup content 

Select the type of data that you want to back up for the SmartStruxure server:

  • All data : Backs up both the historical and configuration databases, which are useful for existing systems. This combined data option protects the configuration, historical data, and custom object type data for a specified date and time.

  • Configuration only : Backs up the configuration database and custom object type data, which are useful for new installations. This data option protects the configuration data for a specified date and time.

Backup set description 

Type a backup comment up to 255 characters that helps identify the type, content, or purpose of the scheduled backup.

  • Backup and Restore Overview
  • Backup Set Properties – Basic Tab
  • No Restore Files Display After Backup
  • Renamed SmartStruxure Server Device Makes Backup Sets Unavailable
  • Incorrect Date Stamp on Backup Set