earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 3.2, 3.3, 2022
15/10/2020

Backup Rule Properties – Basic Tab

Use the Basic tab to view the properties of the backup rule that you create. You can also add a description to help identify the purpose of the backup rule.

 
action_zoom_plus_stroke Basic tab
Figura: Basic tab

Tabla: Basic Tab

Component

Description

Backup content

Select the type of data that you want to back up.

Backup set description

Type a description up to 255 characters that helps to identify the type and contents of the scheduled backup.

Enabled

Select Yes to enable the backup rule.

Lead rule

Enter a backup rule that can act as a lead backup rule.

  • Scheduled Backups
  • General Information Properties – Basic Tab
  • References Tab