earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 2.0, 2.1, 3.0, 3.1
2018/10/24

Backup Rule Properties – Basic Tab

Use the Basic tab to view the properties of the backup rule that you create. You can also add a description to help identify the purpose of the backup rule.

 
action_zoom_plus_stroke Basic tab
图: Basic tab

表格: Basic Tab

Component

Description

Backup content

Select the type of data that you want to back up.

Backup set description

Type a description up to 255 characters that helps to identify the type and contents of the scheduled backup.

Enabled

Select Yes to enable the backup rule.

Lead rule

Enter a backup rule that can act as a lead backup rule.

  • Scheduled Backups
  • General Information Properties – Basic Tab
  • References Tab