Funkcje: Podstawowa funkcjonalność
Wersja produktu: 3.2, 3.3, 2022
2020-10-15

Backup Rules View

Use the Backup rules view to add, edit, or remove backup rules. You can also modify the backup schedule associated with the backup rule. In addition, you can select a backup rule that can act as a lead rule.

 
action_zoom_plus_stroke Backup rules view
Rysunek: Backup rules view

Tabela: Backup Rules View

Number

Description

 
action_zoom_plus_stroke

Use the Backup Rules toolbar to create, edit, or remove backup sets. Więcej informacji zawiera Backup Rules Toolbar .

 
action_zoom_plus_stroke

Use the Backup Rules list to modify backup schedules or set up lead rules. Więcej informacji zawiera Backup Rules List .

  • Backup Rules Toolbar
  • Backup Rules List