earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 2024, 7.0
2024/12/3

Backup Rules View

Use the Backup rules view to add, edit, or remove backup rules. You can also modify the backup schedule associated with the backup rule. In addition, you can select a backup rule that can act as a lead rule.

 
action_zoom_plus_stroke Backup rules view
图: Backup rules view

表格: Backup Rules View

Number

Description

 
action_zoom_plus_stroke

Use the Backup Rules toolbar to create, edit, or remove backup sets. 有关更多信息,请参阅 Backup Rules Toolbar .

 
action_zoom_plus_stroke

Use the Backup Rules list to modify backup schedules or set up lead rules. 有关更多信息,请参阅 Backup Rules List .

  • Backup Rules Toolbar
  • Backup Rules List