earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 3.2, 3.3, 2022
15/10/2020

Backup Rules

The EcoStruxure Building Operation scheduled backups are managed by backup rules, which are conditions that govern behavior. Similar to a scheduled task, a backup rule performs a backup on an EcoStruxure BMS server using three pieces of data: when the backup occurs, what type of data will be backed up, and a comment describing the purpose of the backup.

The EcoStruxure Building Operation software automatically backs up all data on an EcoStruxure BMS server every Sunday at 01:00. However, you can change the backup rule settings. For example, you can change the type of data you want to back up.

You can create your own backup rules to complete different tasks on different EcoStruxure BMS servers. For example, you can create a backup rule that backs up all data on the Enterprise Server twice a day rather than once a week based on the default setting. In addition, you can set up another backup rule for one EcoStruxure BMS server, which acts as the lead, to manage a recurring backup for a group of EcoStruxure BMS servers. Para obtener más información, consulte Backup Rules View .

  • Backup Rules View