Building Operation includes a digital schedule that is combined with a default backup rule. Using this schedule and rule, the system automatically backs up all data on a SmartStruxure server every Sunday at 01:00. You can change the schedule settings for this backup rule, but you cannot delete the schedule and select another.
You can create a custom backup rule and then modify its schedule. For example, you can create a backup rule that backs up all data on an Automation Server daily at 02:00. For more information, see Backup Rules View .