earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 2.0, 2.1, 3.0, 3.1
2019/11/12

Backup Schedules

The EcoStruxure Building Operation database includes a digital schedule that is combined with a default backup rule. Using this schedule and rule, the system automatically backs up all data on an EcoStruxure BMS server every Sunday at 01:00. You can edit the schedule settings for this backup rule, but you cannot delete the schedule and select another.

有关更多信息,请参阅 Editing a Backup Schedule .

重要:

If the automatically scheduled backup occurs during a Daylight Savings Time transition, the backup will not occur. To prevent loss of data, change the scheduled backup to a time that does not conflict with your region's Daylight Savings Time transition.

 
action_zoom_plus_stroke Backup on a standalone SmartX server
图: Backup on a standalone SmartX server

You can create a custom backup rule and then modify its schedule. For example, you can create a backup rule that backs up all data on a SmartX server daily at 02:00.

有关更多信息,请参阅 Creating a Backup Rule .

  • Creating a Backup Rule
  • Editing a Backup Schedule
  • Editing a Backup Schedule
  • Backup Rules View