Funkcje: Podstawowa funkcjonalność
Wersja produktu: 3.2, 3.3, 2022
2020-10-15

Backup Set Properties – Basic Tab

Use the Basic tab to view a read-only summary of the current backup set information.

 
action_zoom_plus_stroke Basic tab
Rysunek: Basic tab

Tabela: Basic Tab

Component

Description

Server revision 

Displays the software version of the EcoStruxure BMS server at the time the backup took place.

Backup date 

Displays the date and time of the backup set.

Backup content 

Select the type of data that you want to back up.

Server type 

Displays the type of EcoStruxure BMS server that can be restored using this backup set.

  • Backup and Restore Overview
  • Backup Sets
  • Backup Options Dialog Box
  • Control Panel – Backup and Archiving
  • Restore Incomplete Due to Network Connectivity Loss
  • General Information Properties – Basic Tab
  • References Tab