earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface utilisateur

Interface utilisateur


Produits : AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Fonctionnalité de base
Version produit : 2.0, 2.1, 3.0, 3.1
24/10/2018

Backup Status Dialog Box

The Backup Status dialog box displays the progress and status of a manual backup. Once the backup starts, the process cannot be stopped but you can close this informational dialog box at any time.

 
action_zoom_plus_stroke Backup Status dialog box
Figure : Backup Status dialog box

Table : Backup Status Dialog Box

Component

Description

Name

​Displays the name of the object.

Status

Displays the current backup status.

Progress

Displays the progress of the backup.

Déclaration

The Backup Status dialog box does not appear during a scheduled backup. However, you can open the Backup and Restore Manager from the Control Panel on the Tools menu to view the current status of a scheduled backup.

  • Backup and Restore Overview
  • Backup Set Properties – Basic Tab
  • Backup Options Dialog Box
  • No Restore Files Display After Backup
  • Renamed SmartX Server Makes Backup Sets Unavailable
  • Incorrect Date Stamp on Backup Set