earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-P-3, AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 7.0
9/30/2025

Select Object Dialog Box

Use the Select Object dialog box to select objects.

 
action_zoom_plus_stroke Select object dialog box
Figure: Select object dialog box

Table: Select Object Dialog Box

Command

Description

Lock path

Select to lock the path and make it absolute. For more information, see Locked and Unlocked Binding Paths .

Path

Displays the path to the selected object.

  • Locked and Unlocked Binding Paths
  • Select Object and Property Dialog Box