earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Användargränssnitt

Användargränssnitt


Produkter: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funktionaliteter: Grundläggande funktionalitet
Produktversion: 3.2, 3.3, 2022
2020-10-15

Select Object Dialog Box

Use the Select Object dialog box to select objects.

 
action_zoom_plus_stroke Select object dialog box
Figur: Select object dialog box

Tabell: Select Object Dialog Box

Command

Description

Lock path

Select to lock the path and make it absolute. Mer information finns i Locked and Unlocked Binding Paths .

Path

Displays the path to the selected object.

  • Locked and Unlocked Binding Paths
  • Select Object and Property Dialog Box