earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-C, AS-B, Enterprise Server, AS-P, WorkStation, Project Configuration Server, Project Configuration Tool
功能: 时间表
产品版本: 1.8
2016/10/13

Basic View of the Schedule Editor

The Basic view of the Schedule Editor serves as a workspace to plan and design a schedule. You use this editor to create, manage, and display weekly scheduled events and exception events.

You can also display the client time zone and the server time zone in the Basic view. This is convenient if your SmartStruxure server is located in a time zone that is different from the time zone where you are configuring the schedule. 有关更多信息,请参阅 Time Zones .

The following figure displays the schedule of the lights within the building. The weekly events are in green and the exception event in blue. The values of the events are also displayed. Monday, October 21 is an exception event so it does not follow the same scheduled events as the rest of the week. The lights are off all day. For the rest of the week, the lights turn on at 07:00 and turn off at 18:00.

 
action_zoom_plus_stroke Basic view of the Schedule Editor
图: Basic view of the Schedule Editor
  • Schedule Editor Overview
  • Advanced View of the Schedule Editor
  • Time Zones
  • Schedule Colors in WorkStation
  • Schedule Editor ​– Basic View
  • Basic Schedule Editor Toolbar