earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Programaciones
Versión del producto: 2024, 7.0
03/12/2024

Calendar Properties – Basic Tab

Use the ​ Basic tab to display general and status information about the calendar. On this tab, you can reference a lead calendar so you can reuse the events configured in the lead calendar in several shadow calendars.

 
action_zoom_plus_stroke Basic tab
Figura: Basic tab

Tabla: Basic Tab

Component

Description

Value

Displays True when the current date matches the date specified in the calendar entry in the Date List .

Remove past events

Select True if you want to remove calendar entries that are older than 60 days.

Lead object

Select a lead calendar if you are creating a shadow calendar.

  • General Information Properties – Basic Tab
  • References Tab