功能: 警报
产品版本: 1.8
2016/10/13

Change of State Alarms

The change of state alarm monitors the state changes of digital variables. You configure the alarm ​to trigger when the variable changes its state to true or to false.

 
action_zoom_plus_stroke Change of state alarm when the monitored variable goes true
图: Change of state alarm when the monitored variable goes true
 
action_zoom_plus_stroke Change of state alarm when the monitored variable goes false
图: Change of state alarm when the monitored variable goes false

For example, you set up a change of state alarm that monitors a ventilation fan. If the fan breaks or stops working, the alarm is triggered.

You can configure the change of state alarms using shunt variable and time delay. 有关更多信息,请参阅 Alarm Functions .

  • Alarm Types
  • Alarms Overview
  • Alarm Functions
  • Change of State Alarm Properties – Basic Tab
  • Creating a Change of State Alarm