earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Trends
Product version: 1.9
12/14/2016

Change of Value Trend Log Properties

Use the Change of Value Trend Log properties to configure the change of value trend log.

 
action_zoom_plus_stroke Change of value trend log properties
Figure: Change of value trend log properties

Table: Change of Value Trend Log Properties

Property

Description

Status

​Displays the status of the trend log.

Enabled

​Displays True if the trend log is enabled.

Logged variable

Enter the variable that you want to log.

Delta

​Select the minimum value change that triggers a new record.

Activation variable

Enter the variable that is to make the trend log start recording values when the variable is true.

For more information, see Trend Log Activation .

Activation time

Specify the time when the trend log is to start recording values.

For more information, see Trend Log Activation .

Maximum log interval

Select the maximum time that can pass between two recordings regardless of whether the delta value has been exceeded or not.

Log size

Select the number of records to store before old records are overwritten including internal records generated by the trend.

For more information, see Log Record Storage .

Clear when enabled

​Select True to clear the trend log when it is enabled.

  • Change of Value Trend Logs
  • Trend Log Types
  • Configure Dialog Box – Configuration Tab
  • Trend Log Activation
  • Configure Dialog Box – Operation Tab
  • Log Record Storage
  • Trend Log Does Not Start Record Due to the Start Condition
  • Missing Trend Log Records
  • General Information Properties – Basic Tab
  • References Tab