earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AD v2, AD v1
功能: 硬件
产品版本: 3.3, 2022, 2023, 2024, 7.0
2021/7/23

Connecting Advanced Display to a Power Adapter

You connect Advanced Display to a USB power adapter in order to supply Advanced Display with power and to ensure that its battery is charged.

显示更多
action_close

AD v2 uses a wired (USB) connection to communicate with EcoStruxure BMS servers. During installation and commissioning, you can use a wireless access point to establish communication between AD v2 and EcoStruxure BMS servers. AD v2 can be powered either by a AS-P server, AS-B server, or USB power adapter.

Communication over a USB Connection

The preinstalled AD-Link application enables AD v2 to communicate with EcoStruxure BMS servers over a USB connection.

When AD v2 is connected to a AS-P server or AS-B server, AD v2 can be powered by the automation server through the USB cable. The screen must not be turned on constantly because this may drain the battery.

通知

LOSS OF DATA OR POWER

  • Use only USB cables ordered from Schneider Electric.

  • Use only USB cables that are designed for AD.

  • Do not use USB cables that exceed 3 m (10 ft).

Failure to follow these instructions can result in loss of data or power.

 
action_zoom_plus_stroke USB connection to a AS-P server or AS-B server
图: USB connection to a AS-P server or AS-B server

警告 警告

HAZARD OF EXPLOSION OR DEVICE DAMAGE

Use only Samsung-approved power adapters.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

To connect Advanced Display to a power adapter
  1. Insert the USB cable from Advanced Display into the power adapter.

  2. Plug the power adapter into the standard AC power outlet.

You can now turn on Advanced Display.

  • AD v2 Communication and Power
  • AD v1 Communication and Power
  • Installing the AD v2 Tablet and Frame
  • Installing the AD v1 Tablet and Frame
  • AD v1 or AD v2 Does Not Turn On or Battery Does Not Charge