earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: WebStation
功能: 时间表
产品版本: 2024, 7.0
2024/12/3

Editing the Start Time and End Time for a Schedule Event

You edit the start time and end time for a schedule event when the condition changes. You can edit the start time for weekly events and single date exception events.

显示更多
action_close

A weekly event occurs every week for an extended period of time on a regular basis. You can schedule more than one weekly event for each day of the week.

To edit the start time and end time for a schedule event
  1. In WebStation, in the System tree pane, select the schedule with the event you want to edit.

  2. In the Schedule workspace, click the schedule event you want to edit.

  3. In properties dialog box, in the At box, enter the start time.

  4. In the Until box, enter the end time.

  5. Click OK .

  6. Click Save .

  • Weekly Events in WebStation
  • Exception Events in WebStation
  • Schedule Workspace Toolbar
  • Schedule Editor in WebStation
  • Editing a Weekly Event
  • Editing a Single Date Exception Event
  • Schedule Workspace
  • Schedule Event Properties Dialog Box – Weekly View
  • Schedule Event Properties Dialog Box – Single Date Exception View