earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Tool
功能: 本地化
产品版本: 1.9
2016/12/14

Changing the Time Zone of a SmartStruxure Server

You change the time zone of a SmartStruxure server to adjust the UTC offset according to the region where the SmartStruxure server is located.

显示更多
action_close

​The Enterprise Server time and date settings are configured through the operating system settings on which the Enterprise Server is installed. The time zone offset, configured through the Enterprise Server, is added by Building Operation to the UTC time. The Enterprise Server time zone settings are therefore independent of the operating system time zone settings.

 
action_zoom_plus_stroke  The Enterprise Server uses the operating system clock on which the server is installed. Time zone offset and DST are then added by Building Operation to the UTC time.
图: The Enterprise Server uses the operating system clock on which the server is installed. Time zone offset and DST are then added by Building Operation to the UTC time.

To adjust your operating system clock, refer to your manufacturer’s manual for the operating system. The Enterprise Server time zone is configured on the Enterprise Server through WorkStation

注释:

To change the time zone of a SmartStruxure server
  1. In WorkStation, on the Tools menu, click Control Panel .

  2. On the Control Panel toolbar, select the SmartStruxure server.

     
    action_zoom_plus_stroke
  3. Click Network time and time zones .

  4. Select Predefined time zone and then select the time zone ​the SmartStruxure server is located in.

     
    action_zoom_plus_stroke
  5. On the File menu, click Save .

If your time zone is not listed, you can create and configure a custom time zone.

  • Creating a Custom Time Zone of a SmartStruxure Server
  • Synchronizing Time Zone Settings on Multiple SmartStruxure Server Devices
  • Time and Time Zone Configuration in Enterprise Server
  • Enterprise Server – Date & Time View