earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Explicación de procesos

Explicación de procesos


Productos AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 2.0, 2.1, 3.0, 3.1
18/05/2018

Checking the Backup Status of an EcoStruxure BMS Server

You check the backup status of an EcoStruxure BMS server to view its backup status and note the date and time of the last backup.

Mostrar más
action_close

Backup Status displays the statuses of an EcoStruxure BMS server: Ready, Backing up, or Backup succeeded.

If a backup does not succeed, the system displays a default alarm informing you of the backup or EcoStruxure BMS server issue. Para obtener más información, consulte Backup and Restore Alarms .

To check the backup status of an EcoStruxure BMS server
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Backup and Restore Manager .

  4. View the EcoStruxure BMS server backup status or date and time of the last successful backup.

  • Backup Status
  • Control Panel Tab
  • Backup and Restore Manager on the Enterprise Server
  • Backup and Restore Manager on a SmartX Server
  • Checking the Online Status of the SmartX Server