earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 2.0, 2.1, 3.0, 3.1
2018/5/18

Checking the Backup Status of an EcoStruxure BMS Server

You check the backup status of an EcoStruxure BMS server to view its backup status and note the date and time of the last backup.

显示更多
action_close

Backup Status displays the statuses of an EcoStruxure BMS server: Ready, Backing up, or Backup succeeded.

If a backup does not succeed, the system displays a default alarm informing you of the backup or EcoStruxure BMS server issue. 有关更多信息,请参阅 Backup and Restore Alarms .

To check the backup status of an EcoStruxure BMS server
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Backup and Restore Manager .

  4. View the EcoStruxure BMS server backup status or date and time of the last successful backup.

  • Backup Status
  • Control Panel Tab
  • Backup and Restore Manager on the Enterprise Server
  • Backup and Restore Manager on a SmartX Server
  • Checking the Online Status of the SmartX Server