earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funktionaliteter: Larm
Produktversion: 3.2, 3.3, 2022
2022-07-12

Checklists

A checklist is a set of steps that guides the user to which action to take when an alarm is triggered. If an alarm goes to normal state, the corresponding checklist is also reset and each step has to be checked again.

Checklists can be voluntary or mandatory. You can force the user to check each step in the checklist before the alarm can be acknowledged.

  • Alarm Functions
  • Alarms Overview
  • User Actions
  • Alarm Control Panel – Checklists View
  • Configuring Forced User Actions
  • Adding a Checklist to an Alarm
  • Editing a Checklist
  • Creating a Checklist
  • Import and Export of Supporting Objects