功能: 警报
产品版本: 1.8
2016/10/13

Checklists

A checklist is a set of steps that guides the user to which action to take when an alarm is triggered. If an alarm goes to normal state, the corresponding checklist is also reset and each step has to be checked again.

 
action_zoom_plus_stroke Checklist dialog box
图: Checklist dialog box

Checklists can be voluntary or mandatory. You can force the user to check each step in the checklist before the alarm can be acknowledged.

  • Alarm Functions
  • Alarms Overview
  • User Actions
  • Alarm Control Panel – Checklists View
  • Configuring Forced User Action
  • Adding a Checklist to an Alarm
  • Editing a Checklist
  • Creating a Checklist