earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Концепт

Концепт


Продукты: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Функции: Сигналы тревоги
Версия продукта: 2024, 7.0
03.12.2024

Comments

​Use comments to save written information about an alarm. Comments can be added and viewed at any time. A comment is automatically tagged with the user name and a time and date stamp. Useful comments could be the cause of the alarm and how it was taken care of. Information like this can be of great help the next time the same alarm is triggered.

Writing a comment is either voluntary or mandatory. You can configure the alarm so the user is required to write a comment when certain events occur, such as when an alarm is disabled.

When you add a comment to an alarm, an event is created and the comment is added to the Last comment column on the alarm record. Only the last added comment is shown on the alarm record. The last comment is deleted if the alarm goes back to Normal state and then is triggered again.

  • Alarm Functions
  • Alarms Overview
  • User Actions
  • Configuring Forced User Actions
  • Control Panel
  • Adding a Comment to an Alarm
  • Add/Remove Columns Dialog Box (Alarms)