earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
功能: 警报
产品版本: 1.8
2016/10/13

Comments

​Use comments to save written information about an alarm. Comments can be added and viewed at any time. A comment is automatically tagged with the user name and a time and date stamp. Useful comments could be the cause of the alarm and how it was taken care of. Information like this can be of great help the next time the same alarm is triggered.

 
action_zoom_plus_stroke A comment is added to a triggered alarm
图: A comment is added to a triggered alarm

Writing a comment is either voluntary or mandatory. You can configure the alarm so the user is required to write a comment when certain events occur, such as when an alarm is disabled.

  • Alarm Functions
  • Alarms Overview
  • User Actions
  • Configuring Forced User Action
  • Control Panel
  • 在报警中添加备注