earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, WorkStation, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 2024, 7.0
12/3/2024

Configure Dialog Box – Operation Tab

Use the Operation tab to select an object, force and release values, and to check the unforced value.

 
action_zoom_plus_stroke The Operation tab displaying both the forced and unforced value
Figure: The Operation tab displaying both the forced and unforced value

Component

Description

Value

Enter the path of the object you want to select or the value that you want to use to override the value of the property.

Force

Click Force to force a value. For more information, see Forced Values .

Unforce

Click to release the forced value. For more information, see Forced Values .

  • Forced Values
  • Forcing a Value
  • Force and Unforce Buttons
  • Releasing a Forced Value
  • Viewing an Unforced Value
  • Configure Dialog Box – Configuration Tab
  • Multi Trend Log List Series Properties