earth_america
user_standard Anmelden
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Konzept

Konzept


Produkte: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funktionen: Basisfunktionalität
Produktversion: 3.2, 3.3, 2022
15.10.2020

Configure Dialog Box – Configuration Tab

You can configure the unit for a value and force or change values.

 
action_zoom_plus_stroke Using the Configure dialog box and the Configuration tab you can change or set units for values.
Abbildung: Using the Configure dialog box and the Configuration tab you can change or set units for values.

Component

Description

Type

Displays the object type. Read-only

Unit

Displays the Unit. Select to change the unit. Für weitere Informationen siehe Units .

Init value

Displays the Init value.

Reference

Displays the Reference.

Forceable

Select to make the value forcible. Für weitere Informationen siehe Softwareübersteuerte Werte .

Retain level

Select how to handle values for warm start, cold start, system events, and system activities. Für weitere Informationen siehe Retain Level .

Null

Select the Null checkbox, to remove any value of a property. The Null checkbox is available for all properties where the value can be removed. For example, you can remove references from trend logs using the Null checkbox.

Values can be forced to a certain value. The true value from the system is displayed in the Unforced value box.

  • Configure Dialog Box – Operation Tab
  • Object Properties
  • Units
  • Softwareübersteuerte Werte
  • Retain Level
  • Configuring the Retain Level