earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 3.2, 3.3, 2022
10/15/2020

Configure Dialog Box – Configuration Tab

You can configure the unit for a value and force or change values.

 
action_zoom_plus_stroke Using the Configure dialog box and the Configuration tab you can change or set units for values.
Figure: Using the Configure dialog box and the Configuration tab you can change or set units for values.

Component

Description

Type

Displays the object type. Read-only

Unit

Displays the Unit. Select to change the unit. For more information, see Units .

Init value

Displays the Init value.

Reference

Displays the Reference.

Forceable

Select to make the value forcible. For more information, see Forced Values .

Retain level

Select how to handle values for warm start, cold start, system events, and system activities. For more information, see Retain Level .

Null

Select the Null checkbox, to remove any value of a property. The Null checkbox is available for all properties where the value can be removed. For example, you can remove references from trend logs using the Null checkbox.

Values can be forced to a certain value. The true value from the system is displayed in the Unforced value box.

  • Configure Dialog Box – Operation Tab
  • Object Properties
  • Units
  • Forced Values
  • Retain Level
  • Configuring the Retain Level