earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 2023
2022/12/17

Configure Dialog Box – Configuration Tab

You can configure the unit for a value and force or change values.

 
action_zoom_plus_stroke Using the Configure dialog box and the Configuration tab you can change or set units for values.
图: Using the Configure dialog box and the Configuration tab you can change or set units for values.

Component

Description

Type

Displays the object type. Read-only

Unit

Displays the Unit. Select to change the unit. 有关更多信息,请参阅 Units .

Init value

Displays the Init value.

Reference

Displays the Reference.

Forceable

Select to make the value forcible. 有关更多信息,请参阅 强制值的概念 .

Retain level

Select how to handle values for warm start, cold start, system events, and system activities. 有关更多信息,请参阅 Retain Level .

Null

Select the Null checkbox, to remove any value of a property. The Null checkbox is available for all properties where the value can be removed. For example, you can remove references from trend logs using the Null checkbox.

Values can be forced to a certain value. The true value from the system is displayed in the Unforced value box.

  • 配置对话框 – 操作标签
  • Object Properties
  • Units
  • 强制值的概念
  • Retain Level
  • Configuring the Retain Level