Productos AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Tendencias
Versión del producto: 2.0, 2.1, 3.0, 3.1
24/10/2018

Configuring a Change of Value Trend Log

You configure the properties of a change of value trend log to meet the unique needs of your site.

Mostrar más
action_close

​The change of value trend log records the variable each time the difference between the current value and the last log value exceeds the delta. Use the change of value trend log to, for example, record a variable that has an unequal oscillation.

Aviso
  • The change of value trend log is limited to 10 records per second.

  • Do not set the delta too small since this can quickly fill up the trend log.

For example, in the figure below, the change of value trend log records a variable every time the variable exceeds or falls below the delta of 3. The records are printed in a trend chart. Notice that the change of value trend log records the values without any time perspective between the records.

 
action_zoom_plus_stroke Change of value trend log schematic.
Figura: Change of value trend log schematic.

The change of value trend log, which is not a variable triggered trend log, has the function to start log records according to a given start condition. Para obtener más información, consulte Trend Log Activation .

You can configure the maximum log interval in a change of value trend log. The maximum log interval is the maximum time that can elapse between two recordings regardless of whether the value has changed or not. The maximum log interval is calculated from the last actual recording. When the maximum log interval is configured, it bypasses the delta and the recording is triggered when the configured time period has elapsed.

Change of value trend log meter functionality

A change of value trend log can be created with initial meter settings . The change of value trend log supports the meter change command and meter consumption calculation. You can view the last meter change information on the change of value trend log object. Para obtener más información, consulte Función Contador .

To configure a change of value trend log
  1. In WorkStation, in the System Tree pane, select the change of value trend log you want to configure.

  2. On the File menu, click Properties .

  3. In the properties dialog box, click the Basic tab.

  4. Edit the basic properties:

    Tabla: Change of Value Trend Log Properties - Basic Tab

    Property

    Description

    Status

    Displays the status of the trend log.

    Enabled

    Displays True if the trend log is enabled.

    Logged variable

    Enter the variable that you want to log.

    Delta

    Select the minimum value change that triggers a new record.

    Activation variable

    Enter the variable that makes the trend log start recording values when the variable is True .

    Para obtener más información, consulte Trend Log Activation .

    Activation time

    Specify the time when the trend log is to start recording values.

    Para obtener más información, consulte Trend Log Activation .

    Maximum log interval

    Select the maximum time that can pass between two recordings regardless if the delta value has been exceeded or not.

    Log size

    Select the number of records to store before old records are overwritten, including internal records generated by the trend log.

    Para obtener más información, consulte Almacenamiento de entradas en el registro .

    Clear when enabled

    Select True to clear the trend log when it is enabled.

  5. Click the Meter Info tab.

  6. Edit the meter properties:

    Tabla: Meter Info Tab

    Property

    Description

    Is meter log

    Select True if the trend log meter function is active.

    Para obtener más información, consulte Función Contador .

    Meter change time

    Enter the time when the meter was changed.

    Meter change user

    Enter the name of the user account that changed the meter.

    End time

    Enter the time when the old meter was replaced.

    End value

    Enter the value the old meter had when it was replaced.

    Start time

    Enter the time when the new meter was installed.

    Start value

    Enter the value of the new meter when it was installed.

    Meter constant

    Enter the constant of the new meter. If the meter counts in kilo (10 3 ), the constant is 1000.

    Min value

    Enter the first value of the new meter after roll-over.

    Max value

    Enter the last value of the new meter before roll-over.

  7. Click OK .

  • Change of Value Trend Logs
  • Change of Value Trend Log Properties – Basic Tab
  • Configure Dialog Box – Configuration Tab
  • Trend Log Activation
  • Cuadro de diálogo Configurar - Pestaña Operación
  • Almacenamiento de entradas en el registro
  • Función Contador
  • Trend Log Does Not Start Record Due to the Start Condition
  • Missing Trend Log Records