You configure the properties of a manual trend log to meet the unique needs of your site.
In WorkStation, in the System Tree pane, select the manual trend log you want to configure.
On the File menu, click Properties .
In the properties dialog box, click the Basic tab.
Edit the basic properties:
Component |
Description |
Unit |
Enter the unit the trend log stores the records in. |
|
Click to open the configuration dialog box where you configure the property. Więcej informacji zawiera Configure Dialog Box – Configuration Tab . |
Click the Meter Info tab.
Edit the meter properties:
Property |
Description |
Is meter log |
Select True if the trend log meter function is active. Więcej informacji zawiera Meter Function . |
Meter change time |
Enter the time when the meter was changed. |
Meter change user |
Enter the name of the user account that changed the meter. |
End time |
Enter the time when the old meter was replaced. |
End value |
Enter the value the old meter had when it was replaced. |
Start time |
Enter the time when the new meter was installed. |
Start value |
Enter the value of the new meter when it was installed. |
Meter constant |
Enter the constant of the new meter. If the meter counts in kilo (10 3 ), the constant is 1000. |
Min value |
Enter the first value of the new meter after roll-over. |
Max value |
Enter the last value of the new meter before roll-over. |
Click OK .