earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, Enterprise Server, AS-P, WorkStation, Project Configuration Server, Virtual Project Servers
Functionalities: Trends
Product version: 1.8
10/13/2016

Configuring a Meter Trend Log

You configure the properties of a meter trend log to meet the unique needs of your site.

Show More
action_close

​The meter trend log is a variable triggered trend log with extra functionality to seamlessly handle consumption calculations independent of meter rollover or meter exchange.

For more information, see Variable Triggered Trend Logs .

You create and configure meter trend logs using WorkStation.

For example, in the figure below, the meter trend log records a meter the 1st of every month. In the middle of February the meter rolls over to 00000. A chart with meter consumption calculation prints the consumption every month.

 
action_zoom_plus_stroke Meter trend log
Figure: Meter trend log

When physically replacing an old meter with a new one, you have to configure the meter trend log by adding the settings of the old meter and new meter in the Manage replacement of meter dialog box in WorkStation. These settings are the foundation to handle a meter rollover or calculating consumption though meter replacement. For more information, see Manage Replacement of Meter Dialog Box .

 
action_zoom_plus_stroke Manage replacement of meter dialog box where you enter the values of the new and old meter.
Figure: Manage replacement of meter dialog box where you enter the values of the new and old meter.
Note:
  • In order for a meter rollover to be managed correctly in the meter trend log and to ensure logging starts at the correct energy reading value, you enter previous meter and new meter information in the Manage replacement of meter dialog box. For more information, see Managing Replacement of a Meter .

To configure a meter trend log
  1. In WorkStation, in the System Tree pane, click the meter trend log you want to configure.

     
    action_zoom_plus_stroke
  2. Edit the properties:

    Table: Meter Trend Log Properties

    Component

    Description

    Status

    ​Displays the status of the trend log.

    Enabled

    ​Displays True if the trend log is enabled.

    Logged variable

    Enter the variable that you want to log.

    Delta

    ​Select the minimum value change that triggers a new record.

    Trigger variable

    Enter the variable that triggers the trend log to start recording.

    Trigger condition

    ​Select when you want the variable recorded: when trigger variable changes to true, changes to false, or all changes. For more information, see Variable Triggered Trend Logs .

    Log size

    Select the number of records to store before old records are overwritten including internal records generated by the trend.

    For more information, see Log Record Storage .

    Clear when enabled

    ​Select True to clear the trend log when it is enabled.

  3. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Meter Trend Logs
  • Meter Trend Log Properties
  • Configure Dialog Box – Configuration Tab
  • Configure Dialog Box – Operation Tab
  • Variable Triggered Trend Logs
  • Log Record Storage
  • Trend Log Does Not Start Record Due to the Start Condition
  • Missing Trend Log Records