earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 时间表
产品版本: 2.0, 2.1, 3.0, 3.1
2022/4/11

Configuring a Schedule as a Shadow

You configure a schedule as a shadow to synchronize it with a schedule that already contains all weekly events and exception events.

提示:

Schedules cannot refer to a calendar located on another EcoStruxure BMS server. You need to create shadow calendars in all EcoStruxure BMS servers that contain schedules that refer to the calendar. In other words, an exception event in a schedule requires the calendar from which the exception event originated to also be present in the shadow device.

显示更多
action_close

When you configure a schedule that controls events in a single part of a building, you might also want the same events to occur in other areas of the building. You can establish a lead and shadow relationship to synchronize the events in schedules and dates in calendars.

For example, the building might require the same heating and lighting events on all floors. Schedule A controls the events on the first floor, Schedule B on the second floor, and Schedule C on the third floor. Using lead and shadow schedules, you can configure one lead schedule, Schedule A, and reference it throughout the building from Schedules B and C, the shadow schedules. When you create the shadow schedule, you need to create the same schedule type as the lead schedule. For example, if you want to create a shadow schedule and the lead schedule type is an analog schedule, you need to create an analog shadow schedule.

 
action_zoom_plus_stroke Lead and shadow schedules
图: Lead and shadow schedules

You use a lead schedule somewhat like a template. To change a property within the shadow schedules, you make the change within the lead schedule. The changes are then reflected in all of the shadow schedules. Only certain properties of the lead schedule, however, are copied into the shadow schedule depending on the property type. Some properties in a lead schedule, such as name and description, are unique to the lead schedule and are not duplicated in the shadow schedule. Other properties that are not specific to the lead schedule, such as effective period, are always duplicated in the shadow schedule. These principles apply to lead calendars and shadow calendars as well.

EcoStruxure BMS supports lead and shadow schedules where exception events, weekly events, and other configuration properties are duplicated in the shadow schedules.

EcoStruxure BMS also supports lead and shadow calendars where the date list is duplicated in the shadow calendars.

Shadow Schedule Pointing to a Lead Schedule

Consider the following scenario where a lead schedule contains an exception event with another calendar assigned in an Enterprise Server. You then want a shadow schedule to point to this lead schedule in the automation server. To accomplish this, you need to create both the shadow calendar and shadow schedule and point them to the corresponding lead calendar and lead schedule. If you only create a shadow schedule, it will fail to update to the lead schedule.

Combining Lead and Shadow Schedules and Calendars

You may want to combine lead/shadow schedules and calendars. In this scenario, a lead schedule is referenced by one or more shadow schedules, while a lead calendar is referenced by one or more shadow calendars. In addition, the lead schedule has one or more exception events that reference the lead calendar, as shown here.

 
action_zoom_plus_stroke Edit Exception Event
图: Edit Exception Event

Because the Period object property is replicated from the lead schedule to the shadow schedule, the calendar name and path are fixed. As a result, you must ensure that the name of the shadow calendar is identical to the lead calendar and that it exists in the same relative system path from the perspective of the shadow schedule.

For example, you should then perform the following:

  • If the lead schedule and calendar exist in the same folder, ensure that the shadow schedule and calendar also exist in the same folder.

  • If the lead schedule exists in \Folder 1 and the lead calendar exists in \Folder1\Folder2, ensure that the shadow schedule exists in\Folder1 and the shadow calendar in \Folder1\Folder2.

To configure a schedule as a shadow
  1. In WorkStation, in the System Tree pane, select the schedule you want to configure as a shadow.

  2. On the File menu, click Properties .

  3. In the Lead object box, enter the schedule that you want to synchronize the shadow schedule with.

     
    action_zoom_plus_stroke
  4. Click OK .

  • Configuring a Calendar as a Shadow
  • Schedule and Calendar Synchronization