You configure the properties of a variable triggered trend log to meet the unique needs of your site.
In WorkStation, in the System Tree pane, click the variable triggered trend log you want to configure.
Edit the properties:
Component |
Description |
Status |
Displays the status of the trend log. |
Enabled |
Displays True if the trend log is enabled. |
Logged variable |
Enter the variable that you want to log. |
Delta |
Select the minimum value change that triggers a new record. |
Trigger variable |
Enter the variable that triggers the trend log to start recording. |
Trigger condition |
Select when you want the variable recorded: when trigger variable changes to true, changes to false, or all changes. For more information, see Variable Triggered Trend Logs . |
Log size |
Select the number of records to store before old records are overwritten including internal records generated by the trend. For more information, see Log Record Storage . |
Clear when enabled |
Select True to clear the trend log when it is enabled. |
Click the Save button