earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Fonctionnalités : Tendances
Version produit : 3.2, 3.3, 2022
15/10/2020

Configuring a Variable Triggered Trend Log

You configure the properties of a variable triggered trend log to meet the unique needs of your site.

Afficher plus
action_close

​The variable triggered trend log records the variable when the conditions of the associated trigger variable are met. Use this type of trend log when the log interval is scheduled to log monthly or yearly, or when another device is used to trigger the log.

For example, in the figure below, the variable triggered trend log records a variable every time the associated trigger variable, for example, a switch, changes to true. The records are printed in a trend chart. Notice that the variable triggered trend log records the variable without any regard to time or delta.

 
action_zoom_plus_stroke Variable triggered trend log schematic
Figure : Variable triggered trend log schematic

You can configure the trend log to collect data when the trigger value changes to True, changes to False, or All changes.

 
action_zoom_plus_stroke Trigger variable changes to true
Figure : Trigger variable changes to true
 
action_zoom_plus_stroke Trigger variable changes to false
Figure : Trigger variable changes to false
 
action_zoom_plus_stroke Trigger variable all changes
Figure : Trigger variable all changes
Variable triggered trend log meter functionality

A variable triggered trend log can be created with initial meter settings. The variable triggered trend log supports the meter change command and meter consumption calculation. You can view the last meter change information on the variable triggered trend log object. Pour plus d'informations, voir Meter Function .

To configure a variable triggered trend log
  1. In WorkStation, in the System Tree pane, select the variable triggered trend log you want to configure.

  2. On the File menu, click Properties .

  3. In the properties dialog box, click the Basic tab.

  4. Edit the basic properties:

    Table : Variable Triggered Trend Log Properties - Basic Tab

    Component

    Description

    Status

    Displays the status of the trend log.

    Enabled

    Displays True if the trend log is enabled.

    Logged variable

    Enter the variable you want to log.

    Delta

    Select the minimum value change that triggers a new record.

    Trigger variable

    Enter the variable that triggers the trend log to start recording.

    Trigger condition

    Select when you want the variable recorded: when the trigger variable changes to True, changes to False, or at all changes.

    Pour plus d'informations, voir Variable Triggered Trend Logs .

    Log size

    Select the number of records to store before old records are overwritten, including internal records generated by the trend log.

    Pour plus d'informations, voir Log Record Storage .

    Clear when enabled

    Select True to clear the trend log when it is enabled.

  5. Click the Meter info tab.

  6. Edit the meter properties:

    Table : Meter Info Tab

    Property

    Description

    Is meter log

    Select True if the trend log meter function is active.

    Pour plus d'informations, voir Meter Function .

    Meter change time

    Enter the time when the meter was changed.

    Meter change user

    Enter the name of the user account that changed the meter.

    End time

    Enter the time when the old meter was replaced.

    End value

    Enter the value the old meter had when it was replaced.

    Start time

    Enter the time when the new meter was installed.

    Start value

    Enter the value of the new meter when it was installed.

    Meter constant

    Enter the constant of the new meter. If the meter counts in kilo (10 3 ), the constant is 1000.

    Min value

    Enter the first value of the new meter after roll-over.

    Max value

    Enter the last value of the new meter before roll-over.

  7. Click OK .

  • Variable Triggered Trend Logs
  • Variable Triggered Trend Log Properties – Basic Tab
  • Configure Dialog Box – Configuration Tab
  • Variable Triggered Trend Logs
  • Configure Dialog Box – Operation Tab
  • Log Record Storage
  • Meter Function
  • Trend Log Does Not Start Record Due to the Start Condition