You configure the properties of an extended trend log to meet the unique needs of your site.
In WorkStation, in the System Tree pane, select the extended trend log you want to configure.
On the File menu, click Properties .
In the properties dialog box, click the Basic tab.
Edit the basic properties:
Component |
Description |
Monitored trend log |
Enter the path to the trend log you want to transfer records from. |
Unit |
The unit of an extended trend log created from the trend log wizard at the same time as the connected trend log inherits the unit of measurement from the connected trend log. The unit of an extended trend log that is manually connected to a trend log needs to be manually configured to use the same unit of measurement as the connected trend log. |
Smart log |
Select True to optimize the transfer of the monitored trend log to the extended trend log. |
Threshold |
Select the percentage threshold at which the trend log transfers its records to the extended trend log. |
Maximum transfer interval |
Select the maximum length of time that can pass between transfers from the monitored trend log to the extended trend log. |
Transfer trigger variable |
Enter a trigger variable to force a transfer of all records from the trend log to the extended trend log, for example, to generate a complete report. Więcej informacji zawiera Extended Trend Logs . |
Log size |
Select the number of records to store before old records are overwritten, including internal records generated by the trend log. Więcej informacji zawiera Log Record Storage . |
Include in report s |
Select True to include the extended trend log data in reports. |
Click the Meter Info tab.
View the meter properties:
Property |
Description |
Is meter log |
Displays True if the trend log meter function is active. Więcej informacji zawiera Meter Function . |
Meter change time |
Displays the time when the meter was changed. |
Meter change user |
Displays the name of the user account that changed the meter. |
End time |
Displays the time when the old meter was replaced. |
End value |
Displays the value the old meter had when it was replaced. |
Start time |
Displays the time when the new meter was installed. |
Start value |
Displays the value of the new meter when it was installed. |
Meter constant |
Displays the constant of the new meter. If the meter counts in kilo (10 3 ), the constant is 1000. |
Min value |
Displays the first value of the new meter after roll-over. |
Max value |
Displays the last value of the new meter before roll-over. |
Meter properties are only available if the meter properties of the connected trend log are active.
Click OK .