earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Explicación de procesos

Explicación de procesos


Productos Enterprise Server, Software Administrator
Funcionalidades: Ingeniería
Versión del producto: 1.9
22/03/2017

​Configuring Server Port Settings

You configure server HTTP, HTTPS, and TCP ports to define the communication of the different protocols. In Software Administrator, you can configure either the ports of the Enterprise Server.

Mostrar más
action_close

​The Software Administrator installs with the Enterprise Server installation package. You use the Software Administrator to start and stop the server service and configure the ports of the Enterprise Server.

Other server settings, for example e-mail service, time, and time zone settings are configured through WorkStation.

Service

The Enterprise Server runs in the background as a Windows service. You start and stop the server service through the Software Administrator or Windows Service. Before shutting down the server, make sure the stop does not negatively affect your site.

Ports

The Enterprise Server uses HTTP and TCP protocols to communicate with other servers and clients. In the Software Administrator, you configure the port number of each protocol the server listens to when communicating through a specific protocol.

To configure a protocol port number, you first have to stop the running Enterprise Server service.

Aviso

Port changes you have made using Software Administrator are not automatically updated in the Communication view for SmartStruxure servers.

Database Location

In the Software Administrator, you find the path to the location where the Enterprise Server writes and stores data and objects that are created by either the Enterprise Server or the user.

Enterprise Server System Log

The Enterprise Server System log contains events logged by the Enterprise Server. Examples of logged events are start up sequence, port settings, failures, run time, and current server status.

To configure server ports
  1. In Software Administrator , click the tab of the Enterprise Server .

     
    action_zoom_plus_stroke
  2. Click Stop Service .

  3. In the HTTP Port box, ​type the port number that the server listens to when communicating through the Hypertext Transfer Protocol.

  4. In the HTTPS Port box, ​type the port number that the server listens to when communicating through the Hypertext Transfer Secure Protocol.

  5. In the TCP Port box, ​type the port number that the server listens to when communicating through the Transmission Control Protocol.

  6. Click Start Service .

  7. Click OK .

  • Software Administrator
  • Software Administrator – Enterprise Server View
  • Starting Software Administrator