earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Как

Как


Продукты: Enterprise Central, Enterprise Server, Software Administrator
Функции: Разработка
Версия продукта: 2024, 7.0
03.12.2024

​Configuring Server Port Settings

You configure server HTTP, HTTPS, and TCP ports to define the communication of the different protocols. In Software Administrator, you can configure either the ports of the Enterprise Server or Enterprise Central.

Показать больше
action_close

The Software Administrator installs with the Enterprise Server and Enterprise Central installation package. You use the Software Administrator to start and stop the server service and configure the ports of the Enterprise Server and Enterprise Central.

Other server settings, for example e-mail service, time, and time zone settings are configured through WorkStation.

Service

The Enterprise Server and Enterprise Central run in the background as Windows services. You start and stop the server services through the Software Administrator or Windows Service. Before shutting down a server, make sure the stop does not negatively affect your site.

Ports

The Enterprise Server and Enterprise Central use HTTP and TCP protocols to communicate with other servers and clients. In the Software Administrator, you configure the port number of each protocol the server listens to when communicating through a specific protocol.

To configure a protocol port number, you first have to stop the running Enterprise Server or Enterprise Central service.

Примечание

Port changes you have made using Software Administrator are not automatically updated in the Communication view for EcoStruxure BMS servers.

Database Location

In the Software Administrator, you find the path to the location where the Enterprise Server or Enterprise Central write and store data and objects that are created by either the Enterprise Server, Enterprise Central, or the user.

Enterprise Server and Enterprise Central System Logs

The Enterprise Server and Enterprise Central System logs contain events logged by the Enterprise Server or Enterprise Central. Examples of logged events are startup sequence, port settings, failures, run time, and current server status.

To configure server ports
  1. In Software Administrator , click the tab of the Enterprise Server or Enterprise Central .

  2. Click Stop Service .

  3. In the HTTP Port box, ​type the port number that the server listens to when communicating through the Hypertext Transfer Protocol.

  4. In the HTTPS Port box, ​type the port number that the server listens to when communicating through the Hypertext Transfer Secure Protocol.

  5. In the TCP Port box, ​type the port number that the server listens to when communicating through the Transmission Control Protocol.

  6. Click Start Service .

  7. Click OK .

  • Software Administrator
  • Software Administrator – Enterprise Server View
  • Software Administrator – Enterprise Central View
  • Starting Software Administrator