earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: Enterprise Server, Project Configuration Server, Software Administrator
功能: 工程
产品版本: 1.8
2016/10/13

​Configuring Server Port Settings

You configure server HTTP, HTTPS, and TCP ports to define the communication of the different protocols. In Software Administrator, you can configure either the ports of the Enterprise Server or the Project Configuration Server.

显示更多
action_close

​The Software Administrator installs with the Enterprise Server and the Project Configuration Server installation package. You use the Software Administrator to start and stop the servers services and configure the ports of the Enterprise Server, or the Project Configuration Server.

Other server settings, for example e-mail service, time, and time zone settings are configured through WorkStation or WorkStation for Projects.

Service

The Enterprise Server and the Project Configuration Server runs in the background as a Windows service. You start and stop the server services through the Software Administrator or Windows Service. Before shutting down the server, make sure the stop does not negatively affect your site or project.

Ports

The Enterprise Server uses HTTP and TCP protocols to communicate with other servers and clients. The Project Configuration Server uses the HTTPS protocol. In the Software Administrator, you configure the port number of each protocol the servers listens to when communicating through a specific protocol.

To configure a protocol port number, you first have to stop the running Enterprise Server or Project Configuration Server services.

注释:

Port changes you have made using Software Administrator are not automatically updated in the Communication view for SmartStruxure servers.

Database Location

In the Software Administrator, you find the path to the location where the Enterprise Server and the Project Configuration Server writes and stores data and objects that are created by either the Enterprise Server, the Project Configuration Server, or the user.

Enterprise Server System Log

The Enterprise Server System log contains events logged by the Enterprise Server. Examples of logged events are start up sequence, port settings, failures, run time, and current server status.

To configure server ports
  1. In Software Administrator , click the tab of the Enterprise Server or the Project Configuration Server .

     
    action_zoom_plus_stroke
  2. Click Stop Service .

  3. In the HTTP Port box, ​type the port number that the server listens to when communicating through the Hypertext Transfer Protocol.

  4. In the HTTPS Port box, ​type the port number that the server listens to when communicating through the Hypertext Transfer Secure Protocol.

  5. In the TCP Port box, ​type the port number that the server listens to when communicating through the Transmission Control Protocol.

  6. Click Start Service .

  7. Click OK .

  • Software Administrator
  • Software Administrator – Enterprise Server View
  • Software Administrator – Project Configuration Server View
  • Starting Software Administrator