earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 警报
产品版本: 2.0, 2.1, 3.0, 3.1
2018/5/18

Configuring Forced User Actions

You force the user to perform certain actions when working with alarms to ​meet the unique needs of your site.

To configure forced user actions
  1. In WorkStation, in the System Tree pane, select the alarm you want to configure.

  2. In the properties pane, click the User Action tab.

  3. Under Required user action , select the check boxes for Comment , Cause note , and Action note to force the user to act on the listed actions.

  4. In the Changes have been made dialog box, click Yes to save the changes.

  • User Actions
  • Create Alarm Wizard – User Action Page