earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 2.0, 2.1, 3.0, 3.1
2018/10/21

Configuring Purge Settings on an Enterprise Server

You purge outdated backup sets to help reduce the resource constraints on an Enterprise Server. You cannot configure these settings on a SmartX server.

显示更多
action_close

An Enterprise Server or Enterprise Central stores multiple local and remote backup sets. These sets can consume much needed space on the computer running the Enterprise Server or Enterprise Central. To resolve this problem, you can configure the Enterprise Server or Enterprise Central to remove outdated backup sets.

You configure purge settings on an Enterprise Server, rather than SmartX servers. 有关更多信息,请参阅 Backup and Restore Manager on the Enterprise Server .

In a multi-server system with an Enterprise Central, you configure the purge settings on both the Enterprise Central and the Enterprise Servers.

Purge Configuration on an Enterprise Server or an Enterprise Central

You can set the maximum number of local and remote backups that you want to store at a given time on the Enterprise Server or the Enterprise Central. The system compares two values:

  • the maximum number that you configured for the Enterprise Server or the Enterprise Central

  • the date stamp on each stored backup

Whenever a new backup is created, the most recent backup set replaces the most outdated backup set. In other words, the system adds a file and then deletes the oldest file to maintain the maximum number that you configured for the Enterprise server or the Enterprise Central.

Local and Remote Purge Settings

You can manage automatic purging on an Enterprise Server or an Enterprise Central by configuring a maximum number of files to store. There are two purge settings:

  • Local setting for the Enterprise Central or Enterprise Server: The local setting, Number of local backup sets to store , manages the backups stored on an Enterprise Central or Enterprise Server.

  • Global setting for SmartX servers: The global setting, Number of AS backup sets to store , manages all the backups stored on the SmartX servers. You cannot configure each SmartX server separately because the global setting affects all the SmartX servers created under the Enterprise Server.

You can vary the number of local and remote backup sets that you store. For example, you can configure the system to store a maximum of five local backup sets for the Enterprise Server and two remote backup sets for each SmartX server.

Enable/Disable Automatic Purging

By default, the EcoStruxure Building Operation software enables automatic purging for both local (Enterprise Server and Enterprise Central) and remote (SmartX servers) backup sets. However, you can disable this feature to ensure that all manual and scheduled backup sets are automatically stored on the Enterprise Server or Enterprise Central. 有关更多信息,请参阅 Backup and Restore Manager on the Enterprise Server .

To configure purge settings on an Enterprise Server
  1. In WorkStation, in the System Tree pane, select the Enterprise Server or Enterprise Central you want to configure.

  2. Click the Control Panel tab.

  3. In the Backup and archiving area, click Backup and restore manager .

  4. In the Number of Automation Server backup sets to store box, enter the maximum number of backups that the Enterprise Server can store for each SmartX server.

  5. In the Number of local backup sets to store box, enter the maximum number of backup sets that the system can store for the Enterprise Server.

  6. On the File menu, click Save .

  • Automatic Purge of Backup Sets
  • Backup and Restore Manager on the Enterprise Server