You configure the address to License Server so Enterprise Server, WorkStation, or a client tool knows where to find available licenses to activate.
Before a WorkStation or Enterprise Server starts to activate EcoStruxure Building Operation software licenses from a License Server, any demo licenses in use must be removed. For more information, see Removing an EcoStruxure Building Operation Software Demo License .
In License Administrator, click the Licenses server address view.
In the License server address box, type @ and then type the address to the License Server.
The address must begin with an @.
If you use a port other than the default port of 27000, type the port number in front of @. For example, 567@localhost.
Use a semicolon to separate addresses to different License Servers.
Click Save .
Next time a WorkStation, client tool, or Enterprise Server starts, it activates available EcoStruxure Building Operation software licenses from the defined License Server.
The License Server address is configured individually on all WorkStations and Enterprise Servers.