earth_america
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Как

Как


Продукты: ​License Administrator, ​License Server
Функции: Управление лицензиями
Версия продукта: 7.0
27.02.2025

Configuring the Address to the License Server

You configure the address to License Server so clients and editors that uses licenses administrated by License Administrator knows where to find available licenses to activate.

Примечание

To configure the address to the License Server
  1. In License Administrator, click the Licenses server address view.

  2. In the License server address box, type @ and then type the address to the License Server.

    Примечание
    • The address must begin with an @.

    • If you use a port other than the default port of 27000, type the port number in front of @. For example, 567@localhost.

    • Use a semicolon to separate addresses to different License Servers.

  3. Click Save .

Next time a client or editor starts, it activates available licenses from the defined License Server.

  • Removing Demo Licenses on License Administrator
  • License Server Address View
  • Unable to Activate EcoStruxure Building Operation Software Licenses