earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: ​License Administrator, ​License Server
功能: 许可证管理
产品版本: 2024, 7.0
2024/12/3

Configuring the Address to the License Server

You configure the address to License Server so Enterprise Server, WorkStation, or a client tool knows where to find available licenses to activate.

注释:

To configure the address to the License Server
  1. In License Administrator, click the Licenses server address view.

  2. In the License server address box, type @ and then type the address to the License Server.

    注释:
    • The address must begin with an @.

    • If you use a port other than the default port of 27000, type the port number in front of @. For example, 567@localhost.

    • Use a semicolon to separate addresses to different License Servers.

  3. Click Save .

Next time a WorkStation, client tool, or Enterprise Server starts, it activates available EcoStruxure Building Operation software licenses from the defined License Server.

注释:
  • The License Server address is configured individually on all WorkStations and Enterprise Servers.

  • Returning EcoStruxure Building Operation Software Demo Licenses Using License Administrator
  • License Server Address View
  • Unable to Activate EcoStruxure Building Operation Software Licenses