Funkcje: Alarmy
Wersja produktu: 3.2, 3.3, 2022
2020-10-15

Configuring the Alarm Message of an Alarm

You configure the text of the alarm message that displays when the alarm is triggered.

To configure the alarm message of an alarm
  1. In WorkStation, in the System Tree pane, select the alarm you want to configure.

  2. In the properties pane, click the Presentation tab.

  3. Under Alarm message , type the alarm message for the different alarm criterias.

  4. In the Changes have been made dialog box, click Yes to save the changes.

  • Create Alarm Wizard – Presentation Page
  • Alarm Messages