Funzionalità: Allarmi
Versione del prodotto: 3.2, 3.3, 2022
22/02/2023

Configuring the Audibility of an Alarm

You configure an alarm to make a sound when it is triggered so that the operator can hear the alarm.

Avviso

In order to grant the correct functioning of alarm sound in combination with acknowledgements, you need to make sure that the Media Feature Pack for your PC Operating System is correctly installed.

Avviso

An alarm sound is only if the selected workspace contains the Alarm pane. Per maggior informazioni, consulta Workspace Components and Customization .

To configure the audibility of an alarm
  1. In WorkStation, in the System Tree pane, select the alarm you want to configure.

  2. Click the Presentation tab.

  3. Select Audible alert to make the alarm sound when it is triggered.

  4. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Alarm Functions
  • Alarms Overview
  • Workspace Components and Customization
  • Configuring the Flashing of an Alarm
  • Configuring the Audibility of an Alarm in Reset State
  • Configuring a Custom Audible Alarm Alert
  • Turning off a Visual and Audible Alert
  • Create Alarm Wizard – Presentation Page