Productos AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
Funcionalidades: Alarmas
Versión del producto: 1.8
13/10/2016

Configuring the Description of an Alarm

You configure the description of an alarm to make it easier to identify the object.

To configure the description of an alarm
  1. In WorkStation, in the System Tree pane, select the alarm you want to configure.

  2. Click the Basic Settings tab.

  3. In the Description box, type a description for the object.

     
    action_zoom_plus_stroke
  4. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Alarm Types
  • Alarms Overview
  • Alarm – Basic Settings View