Funkcje: Alarmy
Wersja produktu: 3.2, 3.3, 2022
2020-10-15

Configuring the Description of an Alarm

You configure the description of an alarm to make it easier to identify the object.

To configure the description of an alarm
  1. In WorkStation, in the System Tree pane, select the alarm you want to configure.

  2. In the properties pane, click the Basic Settings tab.

  3. In the Description box, type a description for the object.

  4. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Alarm Types
  • Alarms Overview
  • Alarm – Basic Settings View